These pragmas can be used to set the section for all declarations below the pragma.
The syntax of the pragmas in C/C++ is:
| #pragma SET_CODE_SECTION ("section name") |
| #pragma SET_DATA_SECTION ("section name") |
In Example 11 x and y are put in the section mydata. To reset the current section to the default used by the compiler, a blank parameter should be passed to the pragma. An easy way to think of the pragma is that it is like applying the CODE_SECTION or DATA_SECTION pragma to all symbols below it.