Example 5. The SECTIONS Directive

/*******************************************************/ /* Sample command file with SECTIONS directive */ /*******************************************************/ file1.obj file2.obj /* Input files */ --output_file=progr.out /* Options */ SECTIONS { .bss : load = RAM .text : load = FLASH .const : load = FLASH .vectors : load = 0xFFE0 { t1.obj (.intvec1) t2.obj (.intvec2) } .data:alpha : align = 16 .data:beta : align = 16 }

Figure 8-2 shows the output sections defined by the SECTIONS directive in Example 5 (.vectors, .text, .const, .bss, .data:alpha, and .data:beta) and shows how these sections are allocated in memory using the MEMORY directive given in Example 3.

Figure 8-2 Section Placement Defined by Example 5secallocate_lau131.gif