MSP430 Assembly
Language Tools
v16.12.0.STS User's Guide
SLAU131N - REVISED DECEMBER 2016
10 Cross-Reference Lister Description
The MSP430 cross-reference lister is a debugging tool. This utility accepts linked object files as input and produces a cross-reference listing as output. This listing shows symbols, their definitions, and their references in the linked source files.
10.1 Producing a Cross-Reference Listing
Figure 10-1 illustrates the steps required to produce a cross-reference listing.
10.2 Invoking the Cross-Reference Lister
To use the cross-reference utility, the file must be assembled with the correct options and then linked into an executable file. Assemble the assembly language files with the --cross_reference option. This option creates a cross-reference listing and adds cross-reference information to the object file. By default, the assembler cross-references only global symbols, but if the assembler is invoked with the --output_all_syms option, local symbols are also added. Link the object files to obtain an executable file.
To invoke the cross-reference lister, enter the following:
| xref430 [options] [input filename [output filename]] |
|
xref430 |
is the command that invokes the cross-reference utility. | |
| options | identifies the cross-reference lister options you want to use. Options are not case sensitive and can appear anywhere on the command line following the command. | |
| -l | (lowercase L) specifies the number of lines per page for the output file. The format of the -l option is -lnum, where num is a decimal constant. For example, -l30 sets the number of lines per page in the output file to 30. The space between the option and the decimal constant is optional. The default is 60 lines per page. | |
| -q | suppresses the banner and all progress information (run quiet). | |
| input filename | is a linked object file. If you omit the input filename, the utility prompts for a filename. | |
| output filename | is the name of the cross-reference listing file. If you omit the output filename, the default filename is the input filename with an .xrf extension. | |
10.3 Cross-Reference Listing Example
These terms defined appear in the cross-reference listing in Example 10-1:
| Symbol | Name of the symbol listed | |
| Filename | Name of the file where the symbol appears | |
| RTYP | The symbol's reference type in this file. The possible reference types are: | |
| STAT | The symbol is defined in this file and is not declared as global. | |
| EDEF | The symbol is defined in this file and is declared as global. | |
| EREF | The symbol is not defined in this file but is referenced as global. | |
| UNDF | The symbol is not defined in this file and is not declared as global. | |
| AsmVal | This hexadecimal number is the value assigned to the symbol at assembly time. A value may also be preceded by a character that describes the symbol's attributes. Table 10-1 lists these characters and names. | |
| LnkVal | This hexadecimal number is the value assigned to the symbol after linking. | |
| DefLn | The statement number where the symbol is defined. | |
| RefLn | The line number where the symbol is referenced. If the line number is followed by an asterisk (*), then that reference can modify the contents of the object. A blank in this column indicates that the symbol was never used. | |
Example 10-1 is an example of cross-reference listing.
Example 10-1 Cross-Reference Listing
MSP430 XREF Utility v3.0.0
2003-2008
File: test.out Tue Mar 18 15:35:55 2008 Page: 1
=============================================================================
MSP430 XREF Utility v3.0.0
2003-2008
File: test.out Tue Mar 18 15:35:55 2008 Page: 2
=============================================================================
Symbol: array
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EDEF -0001 0201 5 2 7
=============================================================================
MSP430 XREF Utility v3.0.0
2003-2008
File: test.out Tue Mar 18 15:35:55 2008 Page: 3
=============================================================================
Symbol: dflag
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EDEF -0000 0200 4 1 10
=============================================================================
MSP430 XREF Utility v3.0.0
2003-2008
File: test.out Tue Mar 18 15:35:55 2008 Page: 4
=============================================================================
Symbol: offset
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EREF 0000 0265 3 8
module2.asm EDEF -0000 0265 4 3 6
=============================================================================
Copyright© 2016, Texas Instruments Incorporated. An IMPORTANT NOTICE for this document addresses availability, warranty, changes, use in safety-critical applications, intellectual property matters and other important disclaimers.