Special Section Types (DSECT, COPY, NOLOAD, NOINIT, and VECT_INIT)

You can assign the following special types to output sections: DSECT, COPY, NOLOAD, NOINIT, and VECT_INIT. These types affect the way that the program is treated when it is linked and loaded. You can assign a type to a section by placing the type after the section definition. For example:

SECTIONS { sec1: load = 0x00002000, type = DSECT {f1.c.obj} sec2: load = 0x00004000, type = COPY {f2.c.obj} sec3: load = 0x00006000, type = NOLOAD {f3.c.obj} sec4: load = 0x00008000, type = NOINIT {f4.c.obj} TIMER0_A1 : { * ( .int53 ) } > INT53 type = VECT_INIT }