Example 19. Linker Command File to Manage Object Components

SECTIONS { UNION { .first: { a1.c.obj(.text), b1.c.obj(.text), c1.c.obj(.text) } load = EMEM, run = PMEM, table(BINIT), table(_first_ctbl) .second: { a2.c.obj(.text), b2.c.obj(.text) } load = EMEM, run = PMEM, table(_second_ctbl) } .extra: load = EMEM, run = PMEM, table(BINIT) ... }

In this example, the output sections .first and .extra are copied from external memory (EMEM) into program memory (PMEM) at boot time while processing the BINIT copy table. After the application has started executing its main thread, it can then manage the contents of the overlay using the two overlay copy tables named: _first_ctbl and _second_ctbl.