| nm430 |
is the command that invokes the name utility. |
| input filename |
is an object file (.obj), executable file (.out), or archive library (.lib). |
| options |
identifies the name utility options you want to use. Options are not case sensitive and can appear anywhere on the command line following the invocation. Precede each option with a hyphen (-). The name utility options are as follows: |
|
--all (-a) |
prints all symbols. |
|
--prep_fname (-f) |
prepends file name to each symbol. |
|
--global (-g) |
prints only global symbols. |
|
--help (-h) |
shows the current help screen. |
|
--format:long (-l) |
produces a detailed listing of the symbol information. |
|
--sort:value (-n) |
sorts symbols numerically rather than alphabetically. |
|
--output (-o)file |
outputs to the given file. |
|
--sort:none (-p) |
causes the name utility to not sort any symbols. |
|
--quiet (-q) |
(quiet mode) suppresses the banner and all progress information. |
|
--sort:reverse (-r) |
sorts symbols in reverse order. |
|
--dynamic (-s) |
lists symbols in the dynamic symbol table for an ELF object module. |
|
--undefined (-u) |
only prints undefined symbols. |