<!-- Start of markdown souce --> As of Code Composer Studio version 9.2.0, the installer command line parameters have changed. Please read the following before using the installer. #### Commandline options for the CCS Installer<br/> |Parameter and Options |Additional Information| |----------------------| ---------------------| |--help|Displays help. Please note, this document contains details that are not available in the installer help.| |--mode unattended| This will install the CCS installer with no GUI interaction. If no other parameters are provided, it will install all product families in the [default directory](#DefaultDir).<br> If this parameter is omitted, the installer will open up in GUI mode and request values for installation.| |--unattendemodeui [none, minimal or minimalWithDialogs]| This option relates to the unattended mode, described above. It is not recommended for standard unattended installs.| |--prefix `<installation directory>`|Where to install CCS. If this parameter is not provided, CCS will be installed to the [default directory](#DefaultDir).| |--optionfile `<filename>`|Parameters for the installer can be added in the optionfile. Please note: The optionfile does not allow for components or product families, those must be passed in on the command line. See [examples](#Examples)| |--enable-components `<comma separated list of product families>`|<p>Product families and their descriptions are listed [below](#ProductFamilies)| |--install-BlackHawk true| This will install BlackHawk debug probes| |--install-Segger true| This will install Segger J-Link debug probes (windows-x64, linux-x64)| <br/> #### <a id="DefaultDir"></a>Default Installation folder<br/> |OS |Default path| |---|------------| |Windows (admin)|C:\ti\ccs`<version>`| |Linux (regular user)|$HOME/ti/ccs`<version>`| |Linux (sudo)|/opt/ti/ccs`<version>`| |OSX (regular user)|$HOME/ti/ccs`<version>`| |OSX (sudo)|/Applications/ti/ccs`<version>`| <br/> #### <a id="ProductFamilies"></a>Installable Product families<br/> |Product family| Description|OS | |----------------------| ---------------------|---| |PF_MSP430|MSP430 ultra-low power MCUs|windows-x64, linux-x64, osx| |PF_MSP432|SimpleLink™ MSP432™ low power + performance MCUs|windows-x64, linux-x64, osx| |PF_CC2X|SimpleLink™ CC13xx and CC26xx Wireless MCUs|windows-x64, linux-x64, osx| |PF_CC3X|SimpleLink™ Wi-Fi® CC32xx Wireless MCUs|windows-x64, linux-x64, osx| |PF_CC2538|CC2538 IEEE 802.15.4 Wireless MCUs|windows-x64, linux-x64, osx| |PF_C28|C2000 real-time MCUs|windows-x64, linux-x64, osx| |PF_TM4C|TM4C12x ARM® Cortex®-M4F core-based MCUs|windows-x64, linux-x64, osx| |PF_PGA|PGA Sensor Signal Conditioners|windows-x64, linux-x64, osx| |PF_HERCULES|Hercules™ Safety MCUs|windows-x64, linux-x64, osx| |PF_SITARA|Sitara™ AMx Processors|windows-x64, linux-x64| |PF_OMAPL|OMAP-L1x DSP + ARM9® Processor|windows-x64, linux-x64| |PF_DAVINCI|DaVinci (DM) Video Processors|windows-x64, linux-x64| |PF_OMAP|OMAP Processors|windows-x64, linux-x64| |PF_TDA_DRA|TDAx Driver Assistance SoCs &amp; Jacinto DRAx Infotainment SoCs|windows-x64, linux-x64| |PF_C55|C55x ultra-low-power DSP|windows-x64, linux-x64| |PF_C6000SC|C6000 Power-Optimized DSP|windows-x64, linux-x64| |PF_C66AK_KEYSTONE|66AK2x multicore DSP + ARM® Processors &amp; C66x KeyStone™ multicore DSP|windows-x64, linux-x64| |PF_MMWAVE|mmWave Sensors|windows-x64, linux-x64| |PF_C64MC|C64x multicore DSP|windows-x64, linux-x64| |PF_DIGITAL_POWER|UCD Digital Power Controllers|windows-x64, linux-x64| <br/> #### <a id="Examples"></a>Examples<br/> ``` ccs_setup_9.2.0.00006.exe --prefix c:\ti\mydir --enable-components PF_MSP430,PF_MSP432 --install-BlackHawk true ``` The example above will install the MSP430 and MSP432 product families of CCS version 9.2.0.00006 in c:\ti\mydir\ccs920. It will also install BlackHawk debug probes. <br/><br/> ``` ccs_setup_9.2.0.00006.bin --prefix $HOME/myinstalldir --enable-components PF_CC2X --mode unattended ``` The example above will install SimpleLink™ CC13xx and CC26xx Wireless MCUs of CCS version 9.2.0.00006 in $HOME/ti/ccs920 without asking the user for any input. <!-- End of markdown source --> <div id="resources" align="center" style="margin-top: 4em; font-size: smaller;"> </div> <div align="center" style="margin-top: 4em; font-size: smaller;"> <a rel="license" href="https://creativecommons.org/licenses/by-nc-nd/4.0/"><img alt="Creative Commons License" style="border-width:0" src="https://software-dl.ti.com/ccs/esd/documents/web_support_v2/cc_license_icon.png" /></a><br />This work is licensed under a <a rel="license" href="https://creativecommons.org/licenses/by-nc-nd/4.0/">Creative Commons Attribution-NonCommercial-NoDerivatives 4.0 International License</a>.</div> <div id="timestamp" align="center" style="margin-top: 4em; font-size: smaller;"> </div>