module ti.uia.events.UIAFrameCtx

UIA Frame Context Instrumentation

The UIAFrameCtx module defines context change events and methods that allow tooling to identify frame context switches and to enable frame-aware filtering, trace and analysis. [ more ... ]
C synopsis target-domain sourced in ti/uia/events/UIAFrameCtx.xdc
DETAILS
The UIAFrameCtx module defines context change events and methods that allow tooling to identify frame context switches and to enable frame-aware filtering, trace and analysis.
It inherits IUIACtx, which defines a function pointer to an isLoggingEnabled function which, if configured to point to a function, will evaluate the function prior to logging the context change event and will determine whether to log the event based on the return value of the function. If the function is not configured, logging will be conditional upon ti_uia_runtime_CtxFilter_module->mIsLoggingEnabled.
The generation of UIAFrameCtx events is also controlled by a module's diagnostics mask, which is described in details in xdc.runtime.Diags. UIAFrameCtx` events are generated only when the Diags.ANALYSIS bit is set in the module's diagnostics mask.
The following configuration script demonstrates how the application might control the logging of ANALYSIS events embedded in the Mod module at configuration time. In this case, the configuration script arranges for the Log statements within modules to always generate ANALYSIS events. Without these configuration statements, no ANALYSIS events would be generated by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
  var Defaults = xdc.useModule('xdc.runtime.Defaults');
  var logger = LoggerSys.create();

  Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
  Defaults.common$.logger = logger;

Example 2: The following example configures a module to support logging of ANALYSIS events, but defers the actual activation and deactivation of the logging until runtime. See the Diags_setMask() function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
  var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var Mod = xdc.useModule('my.pkg.Mod');

  Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
  // turn on logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod+Z");

  // turn off logging of ANALYSIS events in the module
  Diags_setMask("my.pkg.Mod-Z");
 
typedef UIAFrameCtx_IsLoggingEnabledFxn
C synopsis target-domain
typedef Bool (*UIAFrameCtx_IsLoggingEnabledFxn)(Int);
 
 
config UIAFrameCtx_ENABLEMASK  // module-wide

Ctx Filter Enable Mask

C synopsis target-domain
extern const Bits16 UIAFrameCtx_ENABLEMASK;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
 
config UIAFrameCtx_SYNCID  // module-wide

Trace Synchronization ID

C synopsis target-domain
extern const Bits16 UIAFrameCtx_SYNCID;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
 
config UIAFrameCtx_ctxChg  // module-wide

Frame Context Change event

C synopsis target-domain
extern const Log_Event UIAFrameCtx_ctxChg;
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newFrameId
newFrameId — an integer which uniquely identifies the new context
DETAILS
Used to log the start of a new frame If ti_uia_events_UIAFrameCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Context Change event that identifies a new Frame ID
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  Void processFrame(Int frameId){
    ...
    LogCtxChg_frame("New Frame ID=0x%x",frameId);
    ...
  }
This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Frame Ctx Change at Line 123 in demo.c [Prev. Frame ID=0x1234] New Frame ID=0x1235"

 
config UIAFrameCtx_isLoggingEnabledFxn  // module-wide
C synopsis target-domain
extern const IUIACtx_IsLoggingEnabledFxn UIAFrameCtx_isLoggingEnabledFxn;
 
 
UIAFrameCtx_getCtxId()  // module-wide

Get the ID for the current frame

C synopsis target-domain
UInt UIAFrameCtx_getCtxId();
 
RETURNS
returns the frame ID logged by the last call to UIAFrameCtx_logCtxChg.
 
UIAFrameCtx_getEnableOnValue()  // module-wide

Get the EnableOn value

C synopsis target-domain
UInt UIAFrameCtx_getEnableOnValue();
 
RETURNS
returns the App ID value that logging will be enabled for.
 
UIAFrameCtx_isLoggingEnabled()  // module-wide

returns true if the new context matches the value to enable logging with

C synopsis target-domain
Bool UIAFrameCtx_isLoggingEnabled(UInt newFrameId);
 
ARGUMENTS
newFrameId — the new frame ID
DETAILS
Default implementation of the IUIACtx_IsLoggingEnabledFxn for user context. To enable context-aware filtering, in the .cfg script assign UIAFrameCtx_isLoggingEnabledFxn = '&UIAFrameCtx_isLoggingEnabled' or assign your own implementation of this function.
RETURNS
true if logging is enabled
 
UIAFrameCtx_setEnableOnValue()  // module-wide

Set the EnableOn value

C synopsis target-domain
Void UIAFrameCtx_setEnableOnValue(UInt value);
 
ARGUMENTS
value — the CtxId value that logging will be enabled for.
 
UIAFrameCtx_setOldValue()  // module-wide

sets the ti_uia_events_UIAFrameCtx_gLastValue to the new value and returns the old value before it was updated

C synopsis target-domain
UInt UIAFrameCtx_setOldValue(UInt newValue);
 
ARGUMENTS
newValue — the new value to save in the global variable
(return0 the original value of the global variable before it was updated.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId UIAFrameCtx_Module_id();
// Get this module's unique id
 
Bool UIAFrameCtx_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle UIAFrameCtx_Module_heap();
// The heap from which this module allocates memory
 
Bool UIAFrameCtx_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 UIAFrameCtx_Module_getMask();
// Returns the diagnostics mask for this module
 
Void UIAFrameCtx_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/events/UIAFrameCtx.xdc
var UIAFrameCtx = xdc.useModule('ti.uia.events.UIAFrameCtx');
module-wide config parameters
        mask: Diags.ANALYSIS,
        msg: "Frame Ctx Change at %$F [prev. Frame ID=0x%x] %$S"
    };
    UIAFrameCtx.isLoggingEnabledFxn//  = Bool(*)(Int) null;
 
 
 
config UIAFrameCtx.ENABLEMASK  // module-wide

Ctx Filter Enable Mask

Configuration settings
UIAFrameCtx.ENABLEMASK = Bits16 undefined;
 
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags is assigned to control context aware filtering for frame context changes. Must be configured with a value that is 2**SYNCID.
C SYNOPSIS
 
config UIAFrameCtx.SYNCID  // module-wide

Trace Synchronization ID

Configuration settings
UIAFrameCtx.SYNCID = Bits16 undefined;
 
DETAILS
configures the value to be written into the 4 bit context change type field used by the UIASync trace synchronization
C SYNOPSIS
 
config UIAFrameCtx.ctxChg  // module-wide

Frame Context Change event

Configuration settings
UIAFrameCtx.ctxChg = Log.EventDesc {
    mask: Diags.ANALYSIS,
    msg: "Frame Ctx Change at %$F [prev. Frame ID=0x%x] %$S"
};
 
VALUES
fmt — a constant string that describes the context change and provides a format specifier for newFrameId
newFrameId — an integer which uniquely identifies the new context
DETAILS
Used to log the start of a new frame If ti_uia_events_UIAFrameCtx_isLoggingEnabledFxn is not NULL it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Context Change event that identifies a new Frame ID
  #include <ti/uia/runtime/LogCtxChg.h>
  ...
  Void processFrame(Int frameId){
    ...
    LogCtxChg_frame("New Frame ID=0x%x",frameId);
    ...
  }
This event prints the Log call site (%$F) and a format string (%$S) which is recursively formatted with any addition arguments. The following text is an example of what will be displayed for the event:
  "Frame Ctx Change at Line 123 in demo.c [Prev. Frame ID=0x1234] New Frame ID=0x1235"

C SYNOPSIS
 
config UIAFrameCtx.isLoggingEnabledFxn  // module-wide
Configuration settings
UIAFrameCtx.isLoggingEnabledFxn = Bool(*)(Int) null;
 
C SYNOPSIS
 
metaonly config UIAFrameCtx.common$  // module-wide

Common module configuration parameters

Configuration settings
UIAFrameCtx.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 22 Feb 2018 00:30:50 GMT