The UIABenchmark module defines events that allow
tooling to analyze the performance of the software
(processing time, latency, etc.)
The following configuration script demonstrates how the application might
control the logging of ANALYSIS events embedded in the Mod module at configuration
time. In this case, the configuration script arranges for the Log
statements within modules to always generate ANALYSIS events.
Without these configuration statements, no ANALYSIS events would be generated
by any modules.
| config UIABenchmark_start // module-wide |
 |
Benchmark event used to log the start of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'start' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_start, (IArg)"My benchmark event");
The following text will be displayed for the event:
Start: My benchmark event
| config UIABenchmark_startInstance // module-wide |
 |
Benchmark event used to log the start of an operation instance
extern const Log_Event UIABenchmark_startInstance;
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'startInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
| config UIABenchmark_startInstanceWithAdrs // module-wide |
 |
Benchmark event used to log the start of an operation instance
extern const Log_Event UIABenchmark_startInstanceWithAdrs;
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'startInstanceWithAdrs' event along with a task handle as the
instance identifier, the function address and a format string
describing the event.
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void myFunction(){
Task_Handle hTsk = Task_selfMacro();
Log_write3(UIABenchmark_startInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x, fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
...
Log_write3(UIABenchmark_stopInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x", fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
}
The following text will be displayed for the event:
StartInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
StopInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
| config UIABenchmark_startInstanceWithStr // module-wide |
 |
Benchmark event used to log the start of an operation instance
extern const Log_Event UIABenchmark_startInstanceWithStr;
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
str
a constant string reference
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'startInstanceWithStr' event along with a unique instance identifier
and a string reference used only by the pair of start / stop events.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void packetHdlr(Int packetId){
Log_write3(UIABenchmark_startInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
...
Log_write3(UIABenchmark_stopInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
}
The following text will be displayed for the event:
StartInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
StopInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
| config UIABenchmark_stop // module-wide |
 |
Benchmark event used to log the end of an operation
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'stop' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_stop, (IArg)"My benchmark event");
The following text will be displayed for the event:
| config UIABenchmark_stopInstance // module-wide |
 |
Benchmark event used to log the end of an operation instance
extern const Log_Event UIABenchmark_stopInstance;
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'stopInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
| config UIABenchmark_stopInstanceWithAdrs // module-wide |
 |
Benchmark event used to log the end of an operation instance
extern const Log_Event UIABenchmark_stopInstanceWithAdrs;
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
The following C code shows how to log a benchmark
'stopInstanceWithAdrs' event along with a task handle as the
instance identifier, the function address and a format string
describing the event.
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void myFunction(){
Task_Handle hTsk = Task_selfMacro();
Log_write3(UIABenchmark_startInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x, fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
...
Log_write3(UIABenchmark_stopInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x", fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
}
The following text will be displayed for the event:
StartInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
StopInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
| config UIABenchmark_stopInstanceWithStr // module-wide |
 |
Benchmark event used to log the end of an operation instance
extern const Log_Event UIABenchmark_stopInstanceWithStr;
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
str
a constant string reference
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'stopInstanceWithStr' event along with a unique instance identifier
and a string reference used only by the pair of start / stop events.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void packetHdlr(Int packetId){
Log_write3(UIABenchmark_startInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
...
Log_write3(UIABenchmark_stopInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
}
The following text will be displayed for the event:
StartInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
StopInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIABenchmark_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIABenchmark_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIABenchmark_Module_getMask();
// Returns the diagnostics mask for this module
Void UIABenchmark_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| config UIABenchmark.start // module-wide |
 |
Benchmark event used to log the start of an operation
| XDCscript usage |
meta-domain |
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'start' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_start, (IArg)"My benchmark event");
The following text will be displayed for the event:
Start: My benchmark event
C SYNOPSIS
| config UIABenchmark.startInstance // module-wide |
 |
Benchmark event used to log the start of an operation instance
| XDCscript usage |
meta-domain |
msg: "StartInstance: %$S "
};
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'startInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
C SYNOPSIS
| config UIABenchmark.startInstanceWithAdrs // module-wide |
 |
Benchmark event used to log the start of an operation instance
| XDCscript usage |
meta-domain |
msg: "StartInstanceWithAdrs: %$S"
};
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'startInstanceWithAdrs' event along with a task handle as the
instance identifier, the function address and a format string
describing the event.
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void myFunction(){
Task_Handle hTsk = Task_selfMacro();
Log_write3(UIABenchmark_startInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x, fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
...
Log_write3(UIABenchmark_stopInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x", fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
}
The following text will be displayed for the event:
StartInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
StopInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
C SYNOPSIS
| config UIABenchmark.startInstanceWithStr // module-wide |
 |
Benchmark event used to log the start of an operation instance
| XDCscript usage |
meta-domain |
msg: "StartInstanceWithStr: %$S"
};
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
str
a constant string reference
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'startInstanceWithStr' event along with a unique instance identifier
and a string reference used only by the pair of start / stop events.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void packetHdlr(Int packetId){
Log_write3(UIABenchmark_startInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
...
Log_write3(UIABenchmark_stopInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
}
The following text will be displayed for the event:
StartInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
StopInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
C SYNOPSIS
| config UIABenchmark.stop // module-wide |
 |
Benchmark event used to log the end of an operation
| XDCscript usage |
meta-domain |
VALUES
fmt
a constant string that provides format specifiers for up to 7 additional parameters
EXAMPLE
The following C code shows how to log a simple
benchmark 'stop' event along with a user-specified
format string describing the event.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Log_write1(UIABenchmark_stop, (IArg)"My benchmark event");
The following text will be displayed for the event:
C SYNOPSIS
| config UIABenchmark.stopInstance // module-wide |
 |
Benchmark event used to log the end of an operation instance
| XDCscript usage |
meta-domain |
msg: "StopInstance: %$S "
};
VALUES
fmt
a constant string that provides format specifiers for up to 6 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel.
EXAMPLE
The following C code shows how to log a benchmark
'stopInstance' event along with a user-specified
instance identifier and a format string describing the event.
#include <xdc/runtime/Gate.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
static volatile int gMyGlobalInstanceId = 0;
...
IArg key;
int localInstanceId;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
Log_write2(UIABenchmark_startInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
...
Log_write2(UIABenchmark_stopInstance, (IArg)"My benchmark event: instanceId=%d",localInstanceId);
The following text will be displayed for the event:
StartInstance: My benchmark event: instanceId=1
StopInstance: My benchmark event: instanceId=1
C SYNOPSIS
| config UIABenchmark.stopInstanceWithAdrs // module-wide |
 |
Benchmark event used to log the end of an operation instance
| XDCscript usage |
meta-domain |
msg: "StopInstanceWithAdrs: %$S"
};
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
The following C code shows how to log a benchmark
'stopInstanceWithAdrs' event along with a task handle as the
instance identifier, the function address and a format string
describing the event.
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void myFunction(){
Task_Handle hTsk = Task_selfMacro();
Log_write3(UIABenchmark_startInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x, fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
...
Log_write3(UIABenchmark_stopInstanceWithAdrs, (IArg)"My benchmark event: task=0x%x", fnAdrs=0x%x",(IArg)hTsk,(IArg)&myFunc);
}
The following text will be displayed for the event:
StartInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
StopInstanceWithAdrs: My benchmark event: task=0x893230, fnAdrs=0x820060
C SYNOPSIS
| config UIABenchmark.stopInstanceWithStr // module-wide |
 |
Benchmark event used to log the end of an operation instance
| XDCscript usage |
meta-domain |
msg: "StopInstanceWithStr: %$S"
};
VALUES
fmt
a constant string that provides format specifiers for up to 5 additional parameters
instanceId
a unique instance ID that can be used to match benchmark start and stop events
str
a constant string reference
DETAILS
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
EXAMPLE
The following C code shows how to log a benchmark
'stopInstanceWithStr' event along with a unique instance identifier
and a string reference used only by the pair of start / stop events.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIABenchmark.h>
...
Void packetHdlr(Int packetId){
Log_write3(UIABenchmark_startInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
...
Log_write3(UIABenchmark_stopInstanceWithStr, (IArg)"My benchmark event: packetId=0x%x",packetId,(IArg)"(routing)");
}
The following text will be displayed for the event:
StartInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
StopInstanceWithStr: My benchmark event: packetId=0x3bc3 (routing)
Event parameter provides instance data to differentiate
between multiple instances that can run in parallel
C SYNOPSIS
| metaonly config UIABenchmark.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.