This is a GA release of UIA
1.03.00.
The following documentation is available:
Release notes from previous releases are also available in the "docs/relnotes_archive" directory.
ID | Headline |
SDOCM00099710 | Add ARP32 support to UIA |
SDOCM00099548 | UIA should use Timestamp_getFreqMeta() when it becomes available (see SDOCM00099546) |
SDOCM00099543 | UIAMetaData needs config params for timestamp frequency |
SDOCM00099508 | LoggerIdle needs to support writes when buffer is full to get the latest Log data |
SDOCM00099393 | Incorrect timestamp freq displayed for Centaurus devices |
SDOCM00099147 | UIA examples have unnecessary dependency in TREX |
SDOCM00099119 | UIA needs to support GCC for M3/M4/A8/A15 |
SDOCM00098994 | LoggingSetup needs better documentation |
SDOCM00098926 | LoggingSetup configuration should give error when Event upload mode is not supported. |
SDOCM00098925 | UIAMetaData.xs does not get correct clock frequency for Concerto 28x |
SDOCM00098850 | UIA clean up - use module-state variables instead of global variables to avoid OpenMP race conditions |
SDOCM00097947 | LogSync.xs generates invalid rta.xml metadata when auto-creating a sync logger instance of ti.uia.sysbios.LoggerStreamer |
The following table lists dependent product versions and compatibility information. Note that CCS version 5.4 requires XDCTools version 3.25 or higher. If you are using CCS 5.3, you should use XDCTools 3.24.07. This release of UIA requires BIOS 6.35.01 or higher.
CCS Version | XDCTools Version | BIOS Version | NDK Version | IPC Version |
---|---|---|---|---|
5.3 | 3.24.07 | 6.35.01 or higher | 2.22.02.16 or higher | 1.25.01.09 or higher |
5.4 | 3.25 |
The Code Generation tools versions needed with this release of UIA are listed below.
UIA 1.03.00 is backward compatible with the previous 1.02.00 release.
This release supports the following hosts:
Windows XP SP2/SP3
Windows Vista
Linux (Redhat 4 and 5)
ID | Headline |
SDOCM00094008 | Overflow logger not supported for JTAGRUNMODE and NONJTAG_AND_JTAGSTOPMODE |
SDOCM00089387 | UIA has pthread_join which does not work on Andriod |
SDOCM00088803 | Rta/ServiceMgr are not built for C28_float |
SDOCM00087568 | Default LoggingSetup logger buffer sizes are too small - events are always dropped when using JTAGRUNMODE transport |
SDOCM00087567 | Need a way to configure ti.uia.sysbios.LoggingSetup to NOT create an OVERFLOW logger when using JTAGRUNMODE transport |
SDOCM00086708 | ServiceMgr module not configured properly if LoggingSetup.eventUploadMode = JTAGRUNMODE |
SDOCM00084415 | UIA's ServiceMgr's Advanced configuration page does not allow Transport sendFxn to be set |
SDOCM00084411 | Registry name is lost with UIA |
SDOCM00081291 | UploadMode_NONJTAG_AND_JTAGSTOPMODE does not do timestamp correlation |
SDOCM00077654 | UIA Scripts do not support multi-core well |
SDOCM00077653 | Loading DSP on Netra example has lots of warning...but works |
SDOCM00077649 | Rta only obtains events from statically created logger instances |
SDOCM00077589 | IpcMP creates a replyMQ on each processor. It only needs it on the master. |
SDOCM00077588 | IpcMP should not assert in error conditions. It should log an event and recover. |
SDOCM00077586 | Rta's ROV only supports LoggerCircBuf |
SDOCM00077585 | Need to remove all compiler warnings in evmti816x examples |
SDOCM00077324 | ServiceMgr's ROV should obtain information from proxies |
SDOCM00075422 | LoggerCircBuf writes management of the pad is not optimal |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.16_eng or 1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. uia_1_00_00_38.
Subsequent releases of patch upgrades will be identified by the patch number, ex. UIA 1.00.00.26 with directory uia_1_00_00_38. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, contact softwaresupport@ti.com
Last updated: Jan 17, 2013