1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32
33 34 35
36
37 import xdc.runtime.Types;
38 import xdc.runtime.Diags;
39 import ti.uia.events.IUIACtx;
40
41 /*!
42 * UIA User Context Instrumentation
43 *
44 * The UIAUserCtx module provides context change events
45 * and methods that allow tooling to identify user-defined
46 * context switches and to enable context-aware filtering,
47 * trace and analysis.
48 *
49 * It inherits IUIACtx, which defines a function pointer to
50 * an isLoggingEnabled function which, if configured to point to
51 * a function, will evaluate the function prior to logging the context
52 * change event and will store the return value of the function in
53 * ti_uia_runtime_CtxFilter_gIsLoggingEnabled, which is used to
54 * determine whether or not to log events.
55 *
56 * The generation of UIAUserCtx events is also controlled by a module's diagnostics
57 * mask, which is described in details in `{@link xdc.runtime.Diags}`.
58 * `UIAUserCtx` events are generated only when the Diags.ANALYSIS bit is set
59 * in the module's diagnostics mask.
60 *
61 * The following configuration script demonstrates how the application might
62 * control the logging of ANALYSIS events embedded in the `Mod` module at configuration
63 * time. In this case, the configuration script arranges for the `Log`
64 * statements within modules to always generate ANALYSIS events.
65 * Without these configuration statements, no ANALYSIS events would be generated
66 * by any modules.
67 *
68 * @a(Examples)
69 * Example 1: This is part of the XDC configuration file for the application:
70 *
71 * @p(code)
72 * var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
73 * var Diags = xdc.useModule('xdc.runtime.Diags');
74 * var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
75 * var Defaults = xdc.useModule('xdc.runtime.Defaults');
76 * var logger = LoggerSys.create();
77 *
78 * Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
79 * Defaults.common$.logger = logger;
80 * @p
81 *
82 * @p(html)
83 * <hr />
84 * @p
85 *
86 * Example 2: The following example configures a module to support logging
87 * of ANALYSIS events, but defers the actual activation and deactivation of the
88 * logging until runtime. See the `{@link Diags#setMask Diags_setMask()}`
89 * function for details on specifying the control string.
90 *
91 * This is a part of the XDC configuration file for the application:
92 *
93 * @p(code)
94 * var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
95 * var Diags = xdc.useModule('xdc.runtime.Diags');
96 * var Mod = xdc.useModule('my.pkg.Mod');
97 *
98 * Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
99 * @p
100 *
101 * This is a part of the C code for the application:
102 *
103 * @p(code)
104 * // turn on logging of ANALYSIS events in the module
105 * Diags_setMask("my.pkg.Mod+Z");
106 *
107 * // turn off logging of ANALYSIS events in the module
108 * Diags_setMask("my.pkg.Mod-Z");
109 * @p
110 */
111
112 @CustomHeader
113 module UIAUserCtx inherits IUIACtx {
114
115 /*!
116 * ======== ctxChg ========
117 * User-defined Context Change event
118 *
119 * Used to log the start of new state in the user-defined context
120 *
121 * Note that this event should not be referenced directly by user code - it is used
122 * internally by the LogCtxChg_user function, which logs the previous user context Id automatically.
123 *
124 * @a(Example)
125 * The following C code shows how to log a Context Change
126 * event that identifies a new user-specified context ID
127 *
128 * @p(code)
129 * #include <ti/uia/runtime/LogCtxChg.h>
130 * ...
131 * LogCtxChg_user("New user context=0x%x",newUserContextId);
132 * ...
133 *
134 * @p
135 * This event prints the Log call site (%$F) and a format string (%$S)
136 * which is recursively formatted with any addition arguments.
137 * The following text is an example of what will be displayed for the event:
138 * @p(code)
139 * "User Ctx Change at Line 123 in appLoader.c [Prev. ctx = 0x1234] New user context=0x1235"
140 *
141 * @param(fmt) a constant string that describes the context change and provides a format specifier for newAppId
142 * @param(newUserContextId) an integer which uniquely identifies the new user context
143 */
144 config xdc.runtime.Log.Event ctxChg = {
145 mask: Diags.ANALYSIS,
146 msg: "User Ctx Change at %$F [Prev. ctx = 0x%x] %$S"};
147
148 /*!
149 * ======== metaEventUserCtxChg ========
150 * Metadata description of the User Context Change event
151 *
152 * @_nodoc
153 */
154 metaonly config DvtTypes.MetaEventDescriptor metaEventUserCtxChg = {
155 versionId: "2.0",
156 analysisType: DvtTypes.DvtAnalysisType_CONTEXTCHANGE,
157 displayText: "User Ctx Change",
158 tooltipText: "User Context Change",
159 numParameters: 5,
160 paramInfo: [
161 { name: '__FILE__',
162 dataDesc: DvtTypes.DvtDataDesc_FILENAMESTR,
163 dataTypeName: 'String',
164 units: 'none',
165 isHidden: false
166 },
167 { name: '__LINE__',
168 dataDesc: DvtTypes.DvtDataDesc_LINENUM,
169 dataTypeName: 'Int',
170 units: 'none',
171 isHidden: false
172 },
173 { name: 'Prev. User Context',
174 dataDesc: DvtTypes.DvtDataDesc_STATEID,
175 dataTypeName: 'Int',
176 units: 'none',
177 isHidden: false
178 },
179 { name: 'fmt',
180 dataDesc: DvtTypes.DvtDataDesc_FMTSTR,
181 dataTypeName: 'String',
182 units: 'none',
183 isHidden: false
184 },
185 { name: 'New User Context',
186 dataDesc: DvtTypes.DvtDataDesc_STATEID,
187 dataTypeName: 'Int',
188 units: 'none',
189 isHidden: false
190 }]
191
192 };
193 /*!
194 * ======== getCtxId ========
195 * Get the ID for the current user-defined context
196 *
197 * @a(returns)
198 * returns the context ID logged by the last call to UIAUserCtx_logCtxChg.
199 */
200 @Macro Int getCtxId();
201
202 /*!
203 * ======== isLoggingEnabled ========
204 * returns true if the new context matches the value to enable logging with.
205 *
206 * Default implementation of the IUIACtx_IsLoggingEnabledFxn for user context.
207 * To enable context-aware filtering, assign UIAUserCtx_isLoggingEnabledFxn = &UIAUserCtx_isLoggingEnabled
208 * in the config script or programmatically, or assign your own implementation of this
209 * function.
210 * @param(newUserCtx) the new user context
211 * @a(returns) true if logging is enabled
212 */
213 @DirectCall
214 Bool isLoggingEnabled(UInt newUserCtx);
215
216 /*!
217 * ======== setOldValue =========
218 * sets ti_uia_events_UIAUserCtx_gLastValue to the new value and returns the old value before it was updated.
219 *
220 * @param(newValue) the new value to save in the global variable
221 * @a(return) the original value of the global variable before it was updated.
222 */
223 @DirectCall
224 UInt setOldValue(UInt newValue);
225 }
226
227 228 229 230 231