TI-RTOS delivers components that enable engineers to develop applications on Texas Instruments micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. TI-RTOS gives developers a one-stop RTOS solution for developing applications for TI embedded microcontrollers. It provides an OS kernel, communications support, drivers, and more. It is tightly integrated with the Code Composer Studio development environment. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
The following documentation is available:
Click on the links below to view the release notes for the different products.
Examples are provided for the following boards:
To see what has changed in the TI-RTOS Drivers, see the separate TI-Drivers release notes in [as installed]/products/tidrivers_M_mm_pp_bb.
Key | Summary |
---|---|
TIRTOS-509 | tirtos.mak should use same version of tools as in CCS 6.1.3 |
TIRTOS-507 | TIRTOS 2.20 should pick up UIA 2.00.06.52 |
TIRTOS-499 | update IAR/MSP430 to version 6.40 |
TIRTOS-493 | We need to update ‘examples’ directory names in the GSGs |
TIRTOS-478 | Disable semihosting for all GCC/TIRTOS examples |
TIRTOS-473 | Update all RF example to align RF buffers to 4Bytes boundaries. |
TIRTOS-466 | TI-RTOS must update to new MSP43x DriverLib |
TIRTOS-451 | CC3200 examples should define CC32XXWARE |
TIRTOS-435 | Constructed object not shown when pointing ROV at closure with source |
TIRTOS-433 | Add GCC support for the cc13xx/cc26xx examples |
TIRTOS-430 | Add Packet Error Rate example |
TIRTOS-414 | Create standalone example for PDM driver |
TIRTOS-408 | Clock example assumes 1ms Clock.tickPeriod, output is confusing for cc13xx/cc26xx |
TIRTOS-407 | benchloop example should print a message indicating it’s finished |
TIRTOS-397 | Add TMP007 example for all 1350/2650 STK |
TIRTOS-384 | Convert all TIRTOS README .txt files to .md format |
TIRTOS-364 | Add application details/development chapter to Power Mgmt User’s Guide |
TIRTOS-151 | Add support for MSP430FR5994 LaunchPad |
The following is a summary of known compatibility issues from previous releases:
This release requires the following other software components and tools.
All releases have 4 digits (M.mm.pp.bb). This includes GA and engineering releases. Engineering releases are denoted with an _eng suffix (e.g., 2.00.00.15_eng)
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. tirtos_2_00_00_16).
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.01.68 with directory tirtos_1_00_01_68. Typically, these patches only include critical bug fixes.