TI-RTOS delivers components that enable engineers to develop applications on Texas Instruments micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. TI-RTOS gives developers a one-stop RTOS solution for developing applications for TI embedded microcontrollers. It provides an OS kernel, communications support, drivers, and more. It is tightly integrated with the Code Composer Studio development environment. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
The following documentation is provided with this release.
NOTE: Please view the Device Specific driver implementations as they may contain or exclude certain features that are defined in the top level interfaces.
Click on the links below to view the release notes for the different products.
Examples are provided for the following boards:
To see what has changed in the TI-RTOS Drivers, see the separate TI-Drivers release notes in [as installed]/products/tidrivers_M_mm_pp_bb.
Key | Summary |
---|---|
TIRTOS-500 | Update RF examples generated settings to use RF Studio 2.4.0 |
TIRTOS-501 | Import latest CC13xx/CC36xx ccware/driverlib with RF bug fixes |
This release requires the following other software components and tools.
IMPORTANT NOTICE ON CC1350 BLUETOOTH(R) SMART: This TI RTOS release contains a pre-release version of the Bluetooth Smart radio configuration for CC1350. The Bluetooth Smart settings/overrides in this release should not be used in production of CC1350-based products. The CC1350 production-ready Bluetooth Smart settings/overrides are in their final stages of verification, and it should be expected that some radio-specific timings and parameters can change in the production release. This notice does not apply to the Bluetooth Smart settings/overrides for CC2640/50.
All releases have 4 digits (M.mm.pp.bb). This includes GA and engineering releases. Engineering releases are denoted with an _eng suffix (e.g., 2.00.00.15_eng)
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. tirtos_2_00_00_16).
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.01.68 with directory tirtos_1_00_01_68. Typically, these patches only include critical bug fixes.