Texas Instruments Technology for Innovators(tm)

UIA 2.00.05.50 General Availability Release Notes

This release note is divided into the following sections:
Introduction, Documentation, What's New, Dependencies and Compatibility, Host Support, Device Support, Validation Info, Known Issues, Examples, Version Information, Technical Support.

Introduction

This is a GA release of UIA 2.00.05. 

Packages are provided as source code and prebuilt libraries. 

Documentation

The following documentation is available:

Release notes from previous releases are also available in the "docs/relnotes_archive" directory.


What's New

2.00.05.50

Defects Fixed since 2.00.04.46

IDHeadline
SDOCM00119790 SequenceAdjust.java has hardcoded 6 for number of cores
UIA-15 UIA should build libraries with Ethernet support if NDK is found
UIA-16 UIA packages need one line descriptions for cdoc
UIA-17 LoggerIdle ROV has an error when the buffer is wrapped
UIA-19 The LogUC APIs should be controlled by xdc_runtime_Log_DISABLE_ALL

For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory. 

Dependencies and Compatibility

The following table lists dependent product versions and compatibility information.

CCS Version XDCTools Version BIOS Version NDK Version IPC Version
6.0.0 or higher 3.30.00 or higher 6.40.00 or higher 2.22.02.16 or higher 1.25.01.09 or higher

The Code Generation tools versions needed with this release of UIA are listed below.

UIA 2.00.05.50 is backwards compatible with the previous 2.00.04.46 release. 


Host Support

This release supports the following hosts:


Device Support

Expilict Examples
UIA libaries built for

Validation Information

This release was validated using the following components: 

Known Issues

Here are the known issues with this release.

ID Headline
SDOCM00088803 Rta/ServiceMgr are not built for C28_float
SDOCM00087568 Default LoggingSetup logger buffer sizes are too small - events are always dropped when using JTAGRUNMODE transport
SDOCM00086708 ServiceMgr module not configured properly if LoggingSetup.eventUploadMode = JTAGRUNMODE
SDOCM00084415 UIA's ServiceMgr's Advanced configuration page does not allow Transport sendFxn to be set
SDOCM00084411 Registry name is lost with UIA
SDOCM00077654  UIA Scripts do not support multi-core well 
SDOCM00077653  Loading DSP on Netra example has lots of warning...but works
SDOCM00077649  Rta only obtains events from statically created logger instances
SDOCM00077589  IpcMP creates a replyMQ on each processor. It only needs it on the master.
SDOCM00077588  IpcMP should not assert in error conditions. It should log an event and recover.
 SDOCM00077585 Need to remove all compiler warnings in evmti816x examples
 SDOCM00077324 ServiceMgr's ROV should obtain information from proxies


Examples

UIA ships with with several examples that interact with System Analyzer

Single-core

Version Information

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.16_eng or 1.01.00.21-beta).

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. uia_1_00_00_38.

Subsequent releases of patch upgrades will be identified by the patch number, ex. UIA 1.00.00.38 with directory uia_1_00_00_38. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.


Technical Support

For technical support, contact softwaresupport@ti.com

Technical Support and Product Updates


Last updated: Feb 15, 2016