50 #ifndef ti_drivers_sdspi_SDSPIEUSCIA__include
51 #define ti_drivers_sdspi_SDSPIEUSCIA__include
66 #include <ti/sysbios/fatfs/ff.h>
67 #include <ti/sysbios/fatfs/diskio.h>
SDSPIEUSCIA Hardware attributes.
Definition: SDSPIEUSCIA.h:132
SDSPIEUSCIA Object.
Definition: SDSPIEUSCIA.h:152
Definition: SDSPIEUSCIA.h:77
uint32_t pinSCK
Definition: SDSPIEUSCIA.h:137
uint32_t baseAddr
Definition: SDSPIEUSCIA.h:133
uint8_t portMISO
Definition: SDSPIEUSCIA.h:138
uint32_t pinMOSI
Definition: SDSPIEUSCIA.h:141
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
uint8_t clockSource
Definition: SDSPIEUSCIA.h:134
struct SDSPIEUSCIA_Object SDSPIEUSCIA_Object
SDSPIEUSCIA Object.
Definition: SDSPIEUSCIA.h:79
uint32_t pinCS
Definition: SDSPIEUSCIA.h:144
uint32_t bitRate
Definition: SDSPIEUSCIA.h:156
struct SDSPIEUSCIA_Object * SDSPIEUSCIA_Handle
Definition: SDSPIEUSCIA.h:78
SDSPIEUSCIA_CardType
SD Card type inserted.
Definition: SDSPIEUSCIA.h:75
FATFS filesystem
Definition: SDSPIEUSCIA.h:157
SDSPIEUSCIA_CardType cardType
Definition: SDSPIEUSCIA.h:155
struct SDSPIEUSCIA_HWAttrs SDSPIEUSCIA_HWAttrs
uint32_t pinMISO
Definition: SDSPIEUSCIA.h:139
uint8_t portMOSI
Definition: SDSPIEUSCIA.h:140
DSTATUS diskState
Definition: SDSPIEUSCIA.h:154
uint8_t portSCK
Definition: SDSPIEUSCIA.h:136
uint8_t portCS
Definition: SDSPIEUSCIA.h:143
Definition: SDSPIEUSCIA.h:76
uint16_t driveNumber
Definition: SDSPIEUSCIA.h:153
const SDSPI_FxnTable SDSPIEUSCIA_fxnTable