TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Camera.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
104 #ifndef ti_drivers_Camera__include
105 #define ti_drivers_Camera__include
106 
107 #ifdef __cplusplus
108 extern "C" {
109 #endif
110 
111 #include <stdint.h>
112 #include <stddef.h>
113 
125 #define CAMERA_CMD_RESERVED 32
126 
139 #define CAMERA_STATUS_RESERVED -32
140 
147 #define CAMERA_STATUS_SUCCESS 0
148 
155 #define CAMERA_STATUS_ERROR -1
156 
164 #define CAMERA_STATUS_UNDEFINEDCMD -2
165 
169 #define Camera_WAIT_FOREVER ~(0)
170 
174 typedef struct Camera_Config *Camera_Handle;
175 
187 typedef void (*Camera_Callback) (Camera_Handle, void *buf,
188  size_t bufferLength);
189 
196 typedef enum Camera_CaptureMode {
202 
210 
216 typedef enum Camera_HSyncPolarity {
220 
226 typedef enum Camera_VSyncPolarity {
230 
236 typedef enum Camera_PixelClkConfig {
240 
252 typedef enum Camera_ByteOrder {
256 
267 
277 
287 
303 typedef struct Camera_Params {
306 
308  uint32_t outputClock;
309 
312 
315 
318 
321 
324 
327 
330 
332  uint32_t captureTimeout;
333 
336 
338  void *custom;
339 } Camera_Params;
340 
345 typedef void (*Camera_CloseFxn) (Camera_Handle handle);
346 
351 typedef int (*Camera_ControlFxn) (Camera_Handle handle,
352  unsigned int cmd,
353  void *arg);
354 
359 typedef void (*Camera_InitFxn) (Camera_Handle handle);
360 
365 typedef Camera_Handle (*Camera_OpenFxn) (Camera_Handle handle,
366  Camera_Params *params);
367 
372 typedef int (*Camera_CaptureFxn) (Camera_Handle handle,
373  void *buffer, size_t bufferlen);
374 
380 typedef struct Camera_FxnTable {
383 
386 
389 
392 
396 
408 typedef struct Camera_Config {
411 
413  void *object;
414 
416  void const *hwAttrs;
417 } Camera_Config;
418 
428 extern void Camera_close(Camera_Handle handle);
429 
449 extern int Camera_control(Camera_Handle handle, uint32_t cmd, void *arg);
450 
459 extern void Camera_init(void);
460 
481 extern Camera_Handle Camera_open(uint32_t index, Camera_Params *params);
482 
502 extern void Camera_Params_init(Camera_Params *params);
503 
526 extern int Camera_capture(Camera_Handle handle, void *buffer, size_t bufferlen);
527 
528 #ifdef __cplusplus
529 }
530 #endif
531 
532 #endif /* ti_drivers_Camera__include */
Camera_CaptureMode captureMode
Definition: Camera.h:305
Definition: Camera.h:201
Camera_IfSynchoronisation interfaceSync
Definition: Camera.h:323
int(* Camera_ControlFxn)(Camera_Handle handle, unsigned int cmd, void *arg)
A function pointer to a driver specific implementation of Camera_control().
Definition: Camera.h:351
Camera_Callback captureCallback
Definition: Camera.h:335
Camera_VSyncPolarity
Camera VSync polarity.
Definition: Camera.h:226
The definition of a Camera function table that contains the required set of functions to control a sp...
Definition: Camera.h:380
Definition: Camera.h:274
void(* Camera_Callback)(Camera_Handle, void *buf, size_t bufferLength)
The definition of a callback function used by the Camera driver when used in Camera_MODE_CALLBACK.
Definition: Camera.h:187
Definition: Camera.h:227
int(* Camera_CaptureFxn)(Camera_Handle handle, void *buffer, size_t bufferlen)
A function pointer to a driver specific implementation of Camera_capture().
Definition: Camera.h:372
Camera_IfSynchoronisation
Camera interface synchoronisation.
Definition: Camera.h:263
Camera_ControlFxn controlFxn
Definition: Camera.h:385
int Camera_control(Camera_Handle handle, uint32_t cmd, void *arg)
Function performs implementation specific features on a given Camera_Handle.
Camera_FxnTable const * fxnTablePtr
Definition: Camera.h:410
Camera_OpenFxn openFxn
Definition: Camera.h:391
void * custom
Definition: Camera.h:338
Definition: Camera.h:285
Definition: Camera.h:275
Camera_InitFxn initFxn
Definition: Camera.h:388
Definition: Camera.h:264
void Camera_init(void)
Function to initializes the Camera module.
Camera_ByteOrder byteOrder
Definition: Camera.h:320
struct Camera_Config * Camera_Handle
A handle that is returned from a Camera_open() call.
Definition: Camera.h:174
void(* Camera_InitFxn)(Camera_Handle handle)
A function pointer to a driver specific implementation of Camera_init().
Definition: Camera.h:359
Camera_CloseFxn closeFxn
Definition: Camera.h:382
uint32_t outputClock
Definition: Camera.h:308
Camera_ByteOrder
Camera byte order.
Definition: Camera.h:252
Camera_PixelClkConfig
Camera pixel clock configuration.
Definition: Camera.h:236
uint32_t captureTimeout
Definition: Camera.h:332
void Camera_Params_init(Camera_Params *params)
Function to initialize the Camera_Params structure to its defaults.
Camera_StopCaptureConfig
Camera stop capture configuration.
Definition: Camera.h:273
int Camera_capture(Camera_Handle handle, void *buffer, size_t bufferlen)
Function that handles the Camera capture of a frame.
Definition: Camera.h:253
Camera_HSyncPolarity hsyncPolarity
Definition: Camera.h:311
void * object
Definition: Camera.h:413
void(* Camera_CloseFxn)(Camera_Handle handle)
A function pointer to a driver specific implementation of Camera_close().
Definition: Camera.h:345
struct Camera_FxnTable Camera_FxnTable
The definition of a Camera function table that contains the required set of functions to control a sp...
Camera_PixelClkConfig pixelClkConfig
Definition: Camera.h:317
Camera_Handle(* Camera_OpenFxn)(Camera_Handle handle, Camera_Params *params)
A function pointer to a driver specific implementation of Camera_open().
Definition: Camera.h:365
Definition: Camera.h:228
Definition: Camera.h:237
void Camera_close(Camera_Handle handle)
Function to close a Camera peripheral specified by the Camera handle.
Definition: Camera.h:265
Definition: Camera.h:218
struct Camera_Config Camera_Config
Camera Global configuration.
Definition: Camera.h:217
Definition: Camera.h:238
Camera_CaptureFxn captureFxn
Definition: Camera.h:394
Camera_VSyncPolarity vsyncPolarity
Definition: Camera.h:314
void const * hwAttrs
Definition: Camera.h:416
Camera_CaptureMode
Camera capture mode settings.
Definition: Camera.h:196
Camera Global configuration.
Definition: Camera.h:408
Definition: Camera.h:208
struct Camera_Params Camera_Params
Camera Parameters.
Camera Parameters.
Definition: Camera.h:303
Camera_StartCaptureConfig
Camera start capture configuration.
Definition: Camera.h:283
Camera_StopCaptureConfig stopConfig
Definition: Camera.h:326
Definition: Camera.h:284
Camera_StartCaptureConfig startConfig
Definition: Camera.h:329
Definition: Camera.h:254
Camera_Handle Camera_open(uint32_t index, Camera_Params *params)
Function to initialize a given Camera peripheral specified by the particular index value...
Camera_HSyncPolarity
Camera HSync polarity.
Definition: Camera.h:216
Copyright 2015, Texas Instruments Incorporated