![]() |
![]() |
Product | Kernel (SYS/BIOS) | Instrumentation (UIA) | Wired Networking (NDK) | Wireless
Networking |
IPC | Drivers (see Getting Started Guide for more details) | *Ware |
TI-RTOS for C2000 | Included | Included | Included (M3-only) | Included (M3-only) | included | Included (M3-only) | Included (MWare) |
TI-RTOS for MSP43x | Included | Included | Not included | Included | Not included | Included | Included (MSPWare) |
TI-RTOS for TivaC | Included | Included | Included | Included | Not included | Included | Included (TivaWare) |
TI-RTOS for SimpleLink™ Wireless MCUs | Included | Included | Not included | Included | Not included | Included | Included (cc3200-driverlib) |
The following documentation is available:
ID | Headline |
---|---|
SDOCM00114703 | update TI-RTOS simplelink docs overview to have better description and links to CC26xx driverlib docs |
SDOCM00115378 | IAR for ARM compiler tools should move to 7.40.x for CC2650 support |
SDOCM00115634 | MSP432 Power should put TI-RTOS-specific code in a separate library |
SDOCM00115651 | CC3200 Power should check for conflicting user-explicit configuration of Clock or Timestamp proxy |
SDOCM00115733 | I2C_Mode should be taken out of I2C.h and moved into implementation specific .h files |
SDOCM00115822 | remove CC26xx PG 2.0/2.1 driverlib from the product |
SDOCM00116048 | ti.tirtos/package.xs should "loadPackage" ti.drivers.ports.tirtos to work correctly with the "closure" tool |
SDOCM00116106 | SPI driver does not allow MSP432 to reach LPM3 |
SDOCM00116134 | update UARTCC26XX.h and SPICC26XXDMA.h to use new control command definitions |
This release requires the following other software components and tools versions to successfully function:
Product | Supported Targets | Compiler Toolchains | Compiler Versions |
TI-RTOS for C2000 | ti.targets.arm.elf.M3 ti.targets.C28_float ti.targets.C28_large |
Texas Instruments | 5.2.2 (M3) 6.2.5 (C28) |
TI-RTOS for MSP43x | ti.targets.msp430.elf.MSP430X | Texas Instruments | 4.4.2 |
iar.targets.msp430.MSP430X_small | IAR for MSP430 | 5.60.x | |
ti.targets.arm.elf.M4F | Texas Instruments | 5.2.2 | |
iar.targets.arm.M4F | IAR for ARM | 7.40.1 | |
gnu.targets.arm.M4F | GCC (in CCS) | gcc-arm-none-eabi-4_8-2014q3 | |
TI-RTOS for TivaC | ti.targets.arm.elf.M4F iar.targets.arm.M4F gnu.targets.arm.M4F |
Texas Instruments | 5.2.2 |
GCC (in CCS) | gcc-arm-none-eabi-4_8-2014q3 | ||
IAR for ARM | 7.40.1 | ||
TI-RTOS for SimpleLink™ Wireless MCUs | ti.targets.arm.elf.M4 iar.targets.arm.M4 gnu.targets.arm.M4 |
Texas Instruments | 5.2.2 |
GCC (in CCS) | gcc-arm-none-eabi-4_8-2014q3 | ||
IAR for ARM | 7.40.1 |
ID | Severity | Headline |
---|---|---|
SDOCM00099460 | S2 - Major | ping flood causes Concerto board to stop receiving interrupts |
SDOCM00101155 | S2 - Major | usbmsc_SDOCM00100493 fails regression testing (Intermittent spin lock in USB library's USBHCDPipeRead() for LM4F232) |
SDOCM00104253 | S2 - Major | MSP430 Launchpad ez-FET UART emulation issue at buadrate > 28.8kbps |
SDOCM00104686 | S2 - Major | UART in Stellaris launchpad not working above 9600 baud when used with windows apps that use rxtxSerial.dll driver |
SDOCM00106264 | S2 - Major | UART driver doesn't handle RX FIFO overruns. |
SDOCM00107701 | S2 - Major | TI-RTOS filters out BIOS' 64T libraries |
SDOCM00108323 | S2 - Major | TI-RTOS uninstall broke my build environment |
SDOCM00113569 | S2 - Major | Multi-master support for I2C drivers |
SDOCM00115790 | S2 - Major | SPI loopback shows erroneous data for MSP432 |
SDOCM00115853 | S2 - Major | UART_write for CC3200 may retransmit the last character at baudrates > 115200 |
SDOCM00105778 | S3 - Minor | MSP430 UART logging to System Analyzer does not work |
SDOCM00107276 | S3 - Minor | ROV for GPIO exception if opened before Board_initGeneral() is called |
SDOCM00107319 | S3 - Minor | makedef's XDCTOOLS_JAVA_HOME default is bad in supplied examples for stand-alone installer |
SDOCM00107337 | S3 - Minor | BIOS and UIA examples will not link with default MSP430FR5969 linker file. |
SDOCM00107366 | S3 - Minor | Grlibdemo on MSP430FR5969LP not working for IAR |
SDOCM00108264 | S3 - Minor | UIA hello and stairstep examples do not build for some MSP430 devices |
SDOCM00115174 | S3 - Minor | TI-RTOS Makefiles should not use semihosting (or an easy option to enable/disable it) |
SDOCM00115670 | S3 - Minor | TivaC 1294's USB MSC host is really slow |
SDOCM00115875 | S3 - Minor | FatSD raw example for MSP430FR5969 doesn't work in IAR |
SDOCM00115956 | S3 - Minor | Need to look into USB disconnect testing for USB examples |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.15_eng or 1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded inEK-TM4C1294XL the top level directory, ex. tirtos_1_00_01_11.
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.00.68 with directory tirtos_1_00_01_70. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, please refer to the Texas Instruments E2E TI-RTOS Support Forum http://e2e.ti.com/support/embedded/tirtos/default.aspx or other forums in http://e2e.ti.com/ as needed.
Last updated: May 05, 2015