ti-bg December 25, 2013

Network Development Kit (NDK) Software Manifest

Legend

Package Name The name of the application or files
Version Version of the application or files
License Name of the license or licenses that apply to the Package.
Location The directory name and path on the media (or in an archive) where the Package is located.
Delivered As This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive.
Modified This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes.
Obtained from[1] This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded.


Manifest
Package Name Version License Delivered As Modified                                                                            
TI NDK 2.20 BSD Source Y
Location ti/ndk
Obtained from[1] TI



[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.