![]() |
![]() |
This is an General Availability release of TI-RTOS (previously called MCU SDK).
The TI-RTOS delivers components that enable engineers to develop applications on Texas Instruments micro-controller devices. The product is compromised of multiple software components and examples of how to use these components together.The following documentation is available:
ID | Headline |
SDOCM00098482 | need IPv6 support for TI-RTOS tcpEcho example (target and host side apps) |
SDOCM00098023 | Incorrect LED labeling on Stellaris Launchpad board.[c|h] |
SDOCM00097184 | LM4F examples default to 40MHz instead of 80MHz |
SDOCM00096574 | Fixed initialized pointer dereference in USBCDCMOUSE and USBCDCD examples |
SDOCM00095910 | Build error after a build gmake clean |
SDOCM00095695 | Assert_isTrue() does not work in examples |
SDOCM00094212 | I2C ROV needs to show write/read instead of transmit/receive modes |
SDOCM00094118 | Rename product to "TI-RTOS" (not MCUSDK) |
SDOCM00094033 | Windows install is too slow |
SDOCM00087597 | MCU SDK should enhance top-level make to build sub-products (e.g. SYS/BIOS, IPC, etc) |
ID | Headline |
SDOCM00095695 | Assert_isTrue() don't work in examples |
SDOCM00094212 | I2C ROV needs to show write/read instead of transmit/receive modes |
SDOCM00094108 | Missing doxygen information on driver objects |
SDOCM00094053 | MCUSDK sub-products (e.g. UIA, IPC) are not linked into CCS Help |
SDOCM00094026 | Stability issue with USB Host MSC on LM4F232 |
This release requires the following other software components and tools versions to successfully function:
ID | Headline |
SDOCM00098844 | add subcomponent cdoc to the master TI-RTOS cdoc, release notes docs should point to subcomponent docs |
SDOCM00098821 | Add Watchdog_open parameter to specify whether to or not to stall the timer when a breakpoint is hit |
SDOCM00098377 | TI Stellaris launchpad directory/board name should be EK_LM4F120XL and not LM4F120H5QR |
SDOCM00097626 | Giving Priorities to Hwis from TI-RTOS Drivers |
SDOCM00097460 |
No ROV view for USBMSCHFatFs |
SDOCM00095218 |
Available products should show BIOS, NDK and UIA |
SDOCM00094100 | Concerto demo fails when using chrome to enable SD card |
SDOCM00094054 | tcpEcho does not handle more than connections well |
SDOCM00094053 | TI-RTOS sub-products (e.g. UIA, IPC) are not linked into CCS Help |
SDOCM00093967 | MCUSDK Windows install will fail if installed in multiple or single directory that contains more than 38 characters in path |
SDOCM00093268 | Add parity and error checking for UART driver |
SDOCM00090537 | DK-LM3S9D96 fwrite to stdout (console) reports Invalid CIO command. |
SDOCM00088081 | SD Card driver lacks CRC support |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.15_eng or 1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. tirtos_1_00_01_11.
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.00.68 with directory tirtos_1_00_01_70. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, please refer to the Texas Instrument’s E2E BIOS Support Forum http://e2e.ti.com/support/embedded/bios/default.aspx or other forums in http://e2e.ti.com/ as needed.
Last updated: January 28, 2013