package ti.platforms.evm6678

Platform package for the 6678 EVM

XDCspec declarations sourced in ti/platforms/evm6678/package.xdc
requires ti.catalog.c6000;
requires xdc.platform[1, 0, 1];
 
package ti.platforms.evm6678 [1, 0, 0, 0] {
 
    module Platform;
    // Platform support for the evm6678
}
THROWS
XDCException exceptions are thrown for fatal errors. The following error codes are reported in the exception message:
ti.platfoms.evm6678.LINK_TEMPLATE_ERROR
This error is raised when this platform cannot found the default linker command template linkcmd.xdt in the build target's package. When a target does not contain this file, the config parameter xdc.cfg.Program.linkTemplate must be set.
generated on Wed, 27 May 2020 16:22:32 GMT