metaonly interface xdc.tools.product.IProductView |
 |
 |
Define a product as a logical group of RTSC modules
This interface allows a product to define logical groups of RTSC
modules delivered with it. Implementations of this interface are
typically consumed within development environments like IDE's to
render a graphical tree view of the product consisting of these
groups.
[
more ... ]
metaonly interface IProductView { ...
metaonly interface IProductView {
module-wide constants & types
};
module-wide config parameters
module-wide functions
}
DETAILS
This interface allows a product to define logical groups of RTSC
modules delivered with it. Implementations of this interface are
typically consumed within development environments like IDE's to
render a graphical tree view of the product consisting of these
groups.
This is an experimental interface and is subject to change.
struct IProductView.ProductElemDesc |
 |
ProductElemDesc structure
metaonly struct ProductElemDesc {
String elemName;
// Name of group or module
String moduleName;
// Name of module
String iconFileName;
// Icon file name representing element
// Array of ProductElemDesc
};
FIELDS
elemName
Name of element. Elements can be either
groups or modules
moduleName
In case of a leaf node this field will
contain the module name. For intermediate
tree nodes the module name will be set to
null
iconFileName
The name of the icon file that is associated
with this element. In xdctools 3.23, this path
must be relative to the package containing the
IProductView implementation.
In xdctools 3.24.01 (or above), this path may
be relative or absolute. If it's relative,
it's first searched for in the package
containing the IProductView implementation
module and, if this fails, the relative path
is searched via xdc.findFile(). If the icon
is still not found, a default icon will be
used.
elemArray
Array used to define children of a node.
DETAILS
This structure is used to define the logical tree "view" of a
product. This view is composed of elements that are either modules
or groups: modules at the leaves of the tree and groups elsewhere.
config IProductView.homeModule // module-wide |
 |
Top-level module for this product
config String homeModule;
DETAILS
The homeModule is a distinguished "top-level" module that is used
by GUI's as a starting point, or "home page", to navigate to the
other content managed by this product.
config IProductView.linksToArray // module-wide |
 |
Array of IDs of products accessable from this product's home module
config String linksToArray[];
DETAILS
This array of product IDs is used to determine a hierarchical
relationship between products and if a product's modules can be
reached from another product's home page. If product A "links to"
product B, then product B's home page can be closed so long as
product A's home page is open.
IProductView.getProductDescriptor() // module-wide |
 |
Return this product's tree view
DETAILS
This method is typically invoked by development tools like IDE's
to get the product view tree structure.
RETURNS
Returns root node of tree of
ProductElemDesc structures
generated on Tue, 22 May 2018 22:32:56 GMT