1    
     2    /*!
     3     *  ======== ViewXml ========
     4     *  This module sits on top of the ROV core to convert ROV views into
     5     *  XML. This is useful for test scripts and command-line based ROV tools.
     6     */
     7    metaonly module ViewXml {
     8        
     9        /*!
    10         *  ======== processCommand ========
    11         *  This API allows the client to interact with the ROV core and retrieve
    12         *  ROV views.
    13         *
    14         *  It takes String commands of the following forms.
    15         *  1. "lm" - List Modules. 
    16         *     This returns an XML list of all of the modules in the executable's
    17         *     configuration and the views they support.
    18         *  2. "m <module name> <tab name>" - Retrieve tab view for module.
    19         *  3. "cc" - Clear cache.
    20         *     This command clears the ROV core's cache of views. This command
    21         *     should be sent whenever the target state changes.     
    22         */
    23        String processCommand(String cmd);
    24        
    25        /*!
    26         *  ======== listModules ========
    27         *  Returns the list of modules in XML form.
    28         */
    29        String listModules();
    30        
    31        /*!
    32         *  ======== retrieveView ========
    33         *  Retrieves the view in XML form for the given module and tab.
    34         */
    35        String retrieveView(String modName, String tabName);
    36    }
    37    /*
    38     *  @(#) xdc.rov; 1, 0, 1,0; 5-16-2018 11:25:59; /db/ztree/library/trees/xdc/xdc-E04/src/packages/
    39     */
    40