metaonly module xdc.rov.StructureDecoder |
 |
 |
 |
Module for retrieving and decoding target structures
The StructureDecoder is responsible for decoding target data given the
raw target bytes and the data's type as defined in XDC. It also contains
APIs for retrieving data from the target given the data's address.
[
more ... ]
var StructureDecoder = xdc.useModule('xdc.rov.StructureDecoder');
module-wide constants & types
per-instance config parameters
per-instance creation
per-instance functions
DETAILS
The StructureDecoder is responsible for decoding target data given the
raw target bytes and the data's type as defined in XDC. It also contains
APIs for retrieving data from the target given the data's address.
The StructureDecoder relies on the TargetDecoder to decode the raw target
bytes, but is itself responsible for decoding the structure layout. The
decodeStruct API takes as an argument the structure's type representation
in the XDC object model, and refers to this object to determine the size
and offsets of the structure's fields.
The object returned by decodeStruct is not the typed Java representation of
the structure, but rather a typeless JavaScript object which simply
contains all of the same fields. This allows ROV to control the type of the
fields, and specifically to represent arrays as addresses rather than as
objects.
All of the 'decode' methods are essentially private methods. The intended
interface to the StructureDecoder is through the 'fetch' APIs.
struct StructureDecoder.Buffer |
 |
Target buffer
var obj = new StructureDecoder.Buffer;
obj.buffer = Any ...
obj.addr = Int ...
obj.off = Int ...
DETAILS
This structure encapsulates a buffer of target memory (buffer),
the buffer's original target address (addr), and a running offset
into that buffer (off).
Decoding a structure is a recursive process, since the structure may
include fields which are also structures. As StructureDecoder
decodes each field, it updates the off field to move to the next
field.
The original address of the buffer is stored as well so that each
structure field can be given a $addr property with its target
address.
Instance Config Parameters |
 |
var params = new StructureDecoder.Params;
// Instance config-params object
Static Instance Creation |
 |
var params =
new StructureDecoder.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = StructureDecoder.create(Any mem, Any targConfig, params);
// Create an instance-object
DETAILS
The StructureDecoder requires a MemoryImage instance and the target
configuration object from the ROV recap file; i.e.,
recap.build.target.
StructureDecoder.decodeStruct() // instance |
 |
Decode an entire structure by decoding each of the structure's fields
DETAILS
- structType
-
Structure type. Not just a string, it is the XDC object
model representation of the type.
- buffer
-
Buffer of target memory containing raw data.
- inStr
-
Optional structure to fill in. Otherwise decodeStruct will
create a new one.
StructureDecoder.decodeStructArray() // instance |
 |
Decode an array of structures
DETAILS
This API exists to perform some optimizations when decoding an array
of a single type of object.
- structType
-
Structure type of the elements in the array. Not just a
string, it is the XDC object model representation of the
type.
- buffer
-
Buffer of target memory containing raw data.
- len
-
Number of elements in the array.
StructureDecoder.fetchArray() // instance |
 |
Retrieve and decode an array of structures from the target
inst.fetchArray(Any structType, Int addr, Int len, Bool isScalar, Bool addrCheck) returns Any
DETAILS
- structType
-
Structure type. Not just a string, it is the XDC object
model representation of the type.
- addr
-
Target address of the structure to retrieve.
- len
-
Number of entries in the array.
- isScalar
-
Whether it is an array of scalars.
- addrCheck
-
Whether to check the memory read against the section map.
StructureDecoder.fetchStruct() // instance |
 |
Retrieve and decode a structure from the target
inst.fetchStruct(Any structType, Int addr, Bool addrCheck) returns Any
DETAILS
This method retrieves and decodes a structure of the given type at
the given address from the target.
- structType
-
Structure type. Not just a string, it is the XDC object
model representation of the type.
- addr
-
Target address of the structure to retrieve.
- addrCheck
-
Whether to check the memory read against the section map.
generated on Mon, 13 Nov 2017 18:47:53 GMT