metaonly interface xdc.tools.ICmd

Generic xdc-script (xs) command

Modules that implement this interface can serve as "commands" that can be executed from the command line (via xs) or from within XDCscript scripts (without having to fork a separate process to run xs). [ more ... ]
XDCspec summary sourced in xdc/tools/ICmd.xdc
metaonly interface ICmd {  ...
instance:  ...
XDCspec declarations sourced in xdc/tools/ICmd.xdc
package xdc.tools;
 
metaonly interface ICmd {
module-wide config parameters
    config String usage// Usage for this command[] = [ ];
module-wide functions
 
 
instance:
per-instance functions
    Any run// Underlying implementation of the command(Cmdr.Instance cmdr, String args[]);
}
DETAILS
Modules that implement this interface can serve as "commands" that can be executed from the command line (via xs) or from within XDCscript scripts (without having to fork a separate process to run xs).
COMMAND LINE EXAMPLE
The following example runs the xdc.tools.path tool from the command line to get an array of names of all packages below the current working directory (".").
      xs xdc.tools.path -n -a -PR .
XDCSCRIPT EXAMPLE
The following example runs the xdc.tools.path tool from within a script to get an array of names of all packages below the current working directory (".").
      var Main = xdc.module('xdc.tools.path.Main');
      var result = Main.exec(["-n", "-a", "-PR", "."]);
 
config ICmd.usage  // module-wide

Usage for this command

XDCspec declarations sourced in xdc/tools/ICmd.xdc
config String usage[] = [ ];
 
 
ICmd.exec()  // module-wide

xs script entry point

XDCspec declarations sourced in xdc/tools/ICmd.xdc
function exec(args);
 
DETAILS
This function is called from within other XDCscript scripts and performs the same operations as main() except that, rather than output the return value of inst.run(), this value is simply returned to the caller of exec().
 
ICmd.main()  // module-wide

xs shell entry point

XDCspec declarations sourced in xdc/tools/ICmd.xdc
function main(args);
 
DETAILS
This function
  • creates a no-arg instance, inst, of the module inheriting this interface;
  • parses command line arguments placing all options in the config params of the inheriting module;
  • creates a xdc.tools.Cmdr instance, cmdr;
  • calls inst.run() with the cmdr and any command line command line arguments not parsed as options; and
  • outputs the return result from inst.run()
 
ICmd.run()  // instance

Underlying implementation of the command

XDCspec declarations sourced in xdc/tools/ICmd.xdc
Any run(Cmdr.Instance cmdr, String args[]);
 
DETAILS
Since this method is used to support both command line tools and other XDCscript scripts, it is important to avoid explicit termination of the JVM via java.lang.System.exit(); doing so precludes callers from handling failures.
Implementations should instead call
generated on Tue, 21 Feb 2017 01:18:13 GMT