Introduction, License, What's New, Upgrade & Compatibility Information, Host Support, Device Support, Known Issues, Version Information, Technical Support.
RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.
The XDCtools product includes the following components:
XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.
This release of XDCtools is exclusively for use with the MSP430 Grace stand-alone product.
The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.
Package compatibility keys are intended to:
Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:
This release supports the following hosts:
This release is solely for use within the MSP430 Grace stand-alone product.
back to topAll releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.
Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
We encourage you to alert the Grace development team to any issues you may find. Post any issues or questions to the TI E2E forum at: http://www.ti.com/gracefeedback.
Last updated: February 06, 2012 Build Ver: 3.24.00.08 Rev: