Texas Instruments Technology for Innovators(tm)

XDCtools 3.16.00.18 GA Release Notes

October 09, 2009

Introduction, Documentation, License, What's New, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.


Introduction

RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.

The XDCtools product includes the following components:

back to top

Documentation

The product documentation for this release is available in two formats:

Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed on-line at:

Release notes from previous product releases are available in the relnotes_archive directory.

back to top


License

XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.


What's New

The following significant changes are included in 3.16.00.18:


Eclipse Integration Enhancements

The following enhancements have been made in the integration of RTSC with eclipse



Defect history for 3.16.00.18 (This Release)

XDCtools bugs are filed in eclipse bugzilla.

The following defects were resolved in this release:

ID Headline
ECL275983 xgconf does not display xdc.cfg.Program.build
ECL284652 RTSC configuration projects cannot handle project names with periods
ECL284654 The "?" button in the RTSC platform wizard pages is not hooked up to help
ECL285343 xdc.tools.* packages missing summary xdoc
ECL286411 struct initializers can contain mispelled fields
ECL279724 LoggerBuf Basic View should show numEntries and other basic info
ECL290003 Log_print0, etc. cannot be called from control block w/o {}'s
ECL280670 line number info from errors is dropped in eclipse-config
ECL289018 Enum type
ECL285194 coverage profile broken in ti.targets.elf.C64P target
ECL286023 If NULL is passed in place of a params struct, the field 'self' is not correctly initialized
ECL285183 coverage profile broken for ti.targets.arm.elf.* targets
ECL282937 C28x catalogs and platforms should use "code/data" and "page = 0" for most sections

back to top


Upgrade and Compatibility Information

Warning:Starting with XDCtool 2.95, RTSC packages with target content are incompatible with target content from previous releases. Compatibility of meta only content is not affected. Packages with target content would require a recompile. Starting with XDCtool 3.00 release both backward and forward compatibility is maintained for all content.

Package Compatibility Keys

The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.

Package compatibility keys are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:



back to top

Host Support

This release supports the following hosts:

back to top

Dependencies

This release requires the following other software components and tools versions to successfully function:

back to top

Device Support

This release supports the following device families:

back to top

Validation Information

This release was built and validated against using the following components:

back to top


Known Issues

The following major issue is known to exist in this release.

CCSv4 IDE integration not supported on Linux

Command-line operation on Linux is fully supported.

back to top


Version Information

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng or 3.15.01.58-beta).

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.

Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top


Technical Support

Please view and file bugs against this product at rtsc.eclipse.org.

back to top


Last updated: October 09, 2009 Build Ver: 3.16.00.18 Rev: l18