IPC API  3.40.00.06
Data Fields
Mx_Compute Struct Reference

Compute structure. More...

#include <Mx.h>

Collaboration diagram for Mx_Compute:
Collaboration graph

Data Fields

uint32_t coef
 
int key
 
int size
 
uint32_t * inBuf
 
uint32_t * outBuf
 

Detailed Description

Compute structure.

Field Documentation

uint32_t Mx_Compute::coef
int Mx_Compute::key
int Mx_Compute::size
uint32_t* Mx_Compute::inBuf
uint32_t* Mx_Compute::outBuf

The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated