IPC API  3.40.00.06
Data Structures
RcmServer

Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient. More...

Data Structures

struct  RcmServer_FxnDesc
 Function descriptor. More...
 
struct  RcmServer_FxnDescAry
 Function descriptor array. More...
 
struct  RcmServer_ThreadPoolDesc
 Worker pool descriptor. More...
 
struct  RcmServer_ThreadPoolDescAry
 Worker pool descriptor array. More...
 
struct  RcmServer_Params
 RcmServer Instance create parameters. More...
 

Detailed Description

Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient.

Note
With the exception of RcmServer_Params, the RcmServer API is an internal implementation detail of MmServiceMgr and may be changed at will.
Copyright 2015, Texas Instruments Incorporated