Texas Instruments Technology for Innovators(tm)

IPC 3.30.02.13 Report

December 2014

Introduction

This report summarizes results from two software quality assessment tools used to analyze the software in this product:

Unless noted below, all source code, both .c and .h files, for embedded target libraries was analyzed using these tools.


Static Program Analysis Summary

This report summarizes the Static Program Analysis results. For each library, a listing provides:

Click here to view the Static Analysis Report.


MISRA-C:2004 Summary

There are several rules in MISRA-C:2004 that are contrary to long-standing coding standards used in this product, and, hence will not be addressed in the product source code. These rules are listed in the table below. The corresponding checks were explicitly disabled in the tool when the source code was analyzed.

MISRA C Id Brief Summary Exemption Rationale
19.1/A #include statements in a file should only be preceded by other preprocessor directives or comments. Tool reports false positives
19.4/R C macros shall only expand to a braced initialiser, a constant, a parenthesised expression, a type qualifier, a storage class specifier, or a do-while-zero construct. Coding convention
19.6/R #undef shall not be used XDC generated .h files contain #undef
19.7/A A function should not be used in preference to a function-like macro. Coding conventions
19.13/A The # and ## preprocessor operators should not be used. Coding conventions
19.15/R Precautions shall be taken in order to prevent the contents of a header file being included twice. Tool reports false positives
19.17/R All #else, #elif and #endif preprocessor directives shall reside in the same file as the #if or #ifdef directive to which they are related. Tool reports false positives

Click here to view the MISRA-C:2004 Findings Report.

Justification for Not Addressing MISRA-C:2004 Violations