This IPC Release is targeted to SYS/BIOS 6-based platforms.
Introduction, Documentation, What's New, Upgrade Info, Compatibility Information, Device Support, Validation Info, Known Issues, Examples, Version Information, Technical Support.
The IPC product provides software connectivity between multiple processors. Each processor may run either an HLOS (e.g. Linux, QNX) or an RTOS (e.g. SYS/BIOS).
The IPC product is comprised of the following
These components are provided as source code and prebuilt libraries.
The following documentation is available:
In addition, users are encouraged to monitor (and contribute to!) the TI Wiki.
Release notes from previous releases are also available in the relnotes_archive directory.
The following significant changes have been made since 1.25.00
ID | Headline |
SDOCM00102313 | QNX makefiles shouldn't 'install' when only building libs |
SDOCM00102261 | MultiProc names for TCI6636 should match TCI6638 |
SDOCM00102069 | Setting KERNEL_INSTALL_DIR for Keystone fails during MmRpc build |
SDOCM00102315 | QNX multiprocess MessageQ stress tests are failing |
ID | Headline |
SDOCM00102283 | Add support for TCI6636 |
SDOCM00102506 | Update tests to use CMEM directory layout in Linux Utils 4.x |
ID | Headline |
SDOCM00099582 | Mailbox addresses in Benelli driver should be configurable |
ID | Headline |
SDOCM00101856 | Enable slave-side integrators to completely override resource tables |
SDOCM00100157 | Introduce QNX support for OMAP5 |
SDOCM00100360 | Error Handling: When a slave crashes, QNX should detect it and reload the slave |
SDOCM00099748 | On DRA7XX, support SYS/BIOS on IPU1-0 and IPU1-1 (with SYS/BIOS on HOST) |
SDOCM00101582 | Update dependencies to XDC 3.25.01 and BIOS 6.35.02 |
SDOCM00102039 | Introduce QNX support for DRA7XX |
ID | Headline |
SDOCM00098436 | "ti_sdo_ipc_init" section needs to be padded to cacheline size |
SDOCM00098440 | ipc.mak is broken in Windows cmd shell |
SDOCM00098522 | The IPC mailbox drivers for M3 on TI81XX and C6A8149 does not work for SMP BIOS |
ID | Headline |
SDOCM00097544 | Add support for polling for occurrence of interrupts on OMAPL138 |
SDOCM00097853 | Remove ti.sdo.io* content (no longer supported) |
SDOCM00097181 | IPC should provide makefile-based examples |
SDOCM00098543 | Introduce Linux support for TCI6638 |
SDOCM00098458 | Add rproc resource table accessor methods for vring addrs (BIOS-side) |
The IPC packages are available in the "packages/" subdirectory of the product. If you have a previous release of the IPC product, you can install this release next to it, and modify your build scripts/makefiles to use this newer release.
Note, if you're upgrading from a release earlier than IPC 3.00, be sure to review the Upgrade section for each of the releases between your current release and this one. Previous release notes are available in the relnotes_archive directory.
This release supports the following devices (though examples are not provided for all):
This release was built and validated against using the following software components. Please use the versions below, or compatible:
This release was validated using the following hardware platforms:
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipc_3_00_02_26.
Subsequent releases of patch upgrades will be identified by the patch number, e.g. IPC 3.00.01.XX with directory ipc_3_00_01_XX. Typically, these patches only include critical bug fixes.
For technical support, use the community forum TI E2E Community, or email softwaresupport@ti.com.
Check the following web site for updates: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ipc/index.html
Last updated: July 12, 2013