IPC 1.22.04.25 is an GA release of IPC
Interprocess communication mechanisms including message passing, streams, and linked lists, which work transparently in both uniprocessor and muiltiprocessor configurations.
The IPC product is comprised of the following main packages
The following documentation is available:
User Install Guide | |
User Guide (SPRUGO6C) | |
Doxygen API guide | Documents runtime-APIs, type definitions, error codes and constants |
Cdoc API guide | Documents config-time (RTSC) APIs, Asserts and Errors; Indexed and searchable within CCS/Eclipse |
Manifest and License:
IPC Software Manifest and License
Release notes from previous releases are also available in the relnotes_archive directory.
Changes since IPC 1.22.03:
SDOCM00078692 | Ipc_detach skips detaching TransportShmNotify transports |
SDOCM00078694 | NotifyDriverCirc fails after Ipc_detach/attach because receiver has stale data in cache. |
SDOCM00078696 | GateAAMonitor_leave requires int disable around cache freeze/unfreeze |
SDOCM00078739 | There is no check for Notify_intLineRegistered in TransportShmNotifySetup_attach |
For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory.
Interface/API changes:
Most of the APIs in IPC 1.22.01 are compatible with IPC 1.20/1.21. However, code using IPC 1.20/1.21 will have to be recompiled for use with IPC 1.22.01. You must recompile -- relink will not work.
ti.sdo.ipc.* and ti.sdo.utils.* APIs in the IPC 1.2X.XX.XX releases are not compatible with those in the IPC 1.00.0X.XX (GA) release. These APIs have been updated to be consistent with the Linux APIs to share common header files in ti/ipc/. However, APIs in the ti.sdo.io package have not changed since the 1.00 GA release.
OMAP3530 Mailbox assignments swapped
In previous IPC releases, Mailbox 0 was used for DSP-to-ARM notifications and 1 was used for ARM-to-DSP communication. This has been swapped as of IPC 1.22.02. In order for ARM-DSP notifications to work, both the ARM and the DSP must use the same mailbox assignments.
DM8168 MultiProc name changesThe valid MultiProc names for DM8168 were changed in IPC 1.21.02 to match the official names. They are now as follows:
'ti.sdo.ipc.examples.platforms.simDM8168.xxx' sample platforms in IPC have been renamed to 'ti.sdo.ipc.examples.platforms.evmTI816X.xxx'. Applications should use 'evmTI816X' instead of 'simDM8168' if the applications are using the example platforms packaged with IPC. Existing platforms generated using the platform wizard are not affected by this change.
ti.sdo.ipc.family.dm8168 package name changeThe ti.sdo.ipc.family.dm8168 package has been renamed to ti.sdo.ipc.family.ti81xx. Application that use the NotifySetup or InterruptXXX modules contained within must use the new package name in order to build with this version of IPC
This release supports the following hosts:
Windows XP SP2/SP3
Windows Vista
Linux (Redhat 4 and 5)
This release requires the following other software components and tools versions to successfully function:
SDOCM00068256 | The linker will product a warning about "placing code in a data section" when building c6x applications using the whole_program[_debug] build profile for some devices. It is safe to ignore this warning. |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.21.00.01_eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipc_1_21_00_01.
Subsequent releases of patch upgrades will be identified by the patch number, ex. IPC 1.21.00.01 with directory ipc_1_21_00_01. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, use the community forum TI E2E Community, or email softwaresupport@ti.com.
Last updated: February 10, 2011