Setting Default Compiler Options (PRU_C_OPTION)

You might find it useful to set the compiler, assembler, and linker default options using the PRU_C_OPTION environment variable. If you do this, the compiler uses the default options and/or input filenames that you name PRU_C_OPTION every time you run the compiler.

Setting the default options with these environment variables is useful when you want to run the compiler repeatedly with the same set of options and/or input files. After the compiler reads the command line and the input filenames, it looks for the PRU_C_OPTION environment variable and processes it.

The table below shows how to set the PRU_C_OPTION environment variable. Select the command for your operating system:

Operating System Enter
UNIX (Bourne shell) PRU_C_OPTION="option1[option2 . . .]"; export PRU_C_OPTION
Windows set PRU_C_OPTION=option1[option2. . .]

Environment variable options are specified in the same way and have the same meaning as they do on the command line. For example, if you want to always run quietly (the --quiet option), enable C/C++ source interlisting (the --src_interlist option), and link (the --run_linker option) for Windows, set up the PRU_C_OPTION environment variable as follows:

set PRU_C_OPTION=--quiet --src_interlist --run_linker

In the following examples, each time you run the compiler, it runs the linker. Any options following --run_linker on the command line or in PRU_C_OPTION are passed to the linker. Thus, you can use the PRU_C_OPTION environment variable to specify default compiler and linker options and then specify additional compiler and linker options on the command line. If you have set --run_linker in the environment variable and want to compile only, use the compiler --compile_only option. These additional examples assume PRU_C_OPTION is set as shown above:

clpru *c ; compiles and links clpru --compile_only *.c ; only compiles clpru *.c --run_linker lnk.cmd ; compiles and links using a command file clpru --compile_only *.c --run_linker lnk.cmd ; only compiles (--compile_only overrides --run_linker)

For details on compiler options, see Section 2.3. For details on linker options, see the Linker Description chapter in the PRU Assembly Language Tools User's Guide.