Run Length Encoded (RLE) Format

NOTE

This section applies to applications that use EABI only.

8-bit index Initialization data compressed using run length encoding

The data following the 8-bit index is compressed using Run Length Encoded (RLE) format. uses a simple run length encoding that can be decompressed using the following algorithm:

  1. Read the first byte, Delimiter (D).
  2. Read the next byte (B).
  3. If B != D, copy B to the output buffer and go to step 2.
  4. Read the next byte (L).
    1. If L == 0, then length is either a 16-bit, a 24-bit value, or we’ve reached the end of the data, read next byte (L).
      1. If L == 0, length is a 24-bit value or the end of the data is reached, read next byte (L).
        1. If L == 0, the end of the data is reached, go to step 7.
        2. Else L <<= 16, read next two bytes into lower 16 bits of L to complete 24-bit value for L.
      2. Else L <<= 8, read next byte into lower 8 bits of L to complete 16-bit value for L.
    2. Else if L > 0 and L < 4, copy D to the output buffer L times. Go to step 2.
    3. Else, length is 8-bit value (L).
  5. Read the next byte (C); C is the repeat character.
  6. Write C to the output buffer L times; go to step 2.
  7. End of processing.

The run-time support library has a routine __TI_decompress_rle24() to decompress data compressed using RLE. The first argument to this function is the address pointing to the byte after the 8-bit index. The second argument is the run address from the C auto initialization record.

NOTE

RLE Decompression Routine

The previous decompression routine, __TI_decompress_rle(), is included in the run-time-support library for decompressing RLE encodings generated by older versions of the linker.