TMS320C28x Assembly Language
Tools
v18.1.0.LTS User's Guide
SPRU513P - REVISED JANUARY 2018
9 Absolute Lister Description
The TMS320C28x absolute lister is a debugging tool that accepts linked object files as input and creates .abs files as output. These .abs files can be assembled to produce a listing that shows the absolute addresses of object code. Manually, this could be a tedious process requiring many operations; however, the absolute lister utility performs these operations automatically.
9.1 Producing an Absolute Listing
Figure 9-1 illustrates the steps required to produce an absolute listing.
9.2 Invoking the Absolute Lister
The syntax for invoking the absolute lister is:
| abs2000 [-options] input file |
| abs2000 | is the command that invokes the absolute lister. | |
| options | identifies the absolute lister options that you want to use. Options are not case sensitive and can appear anywhere on the command line following the command. Precede each option with a hyphen (-). The absolute lister options are as follows: | |
| -e | enables you to change the default naming conventions for filename extensions on assembly files, C source files, and C header files. The valid options are:
|
|
| The . in the extensions and the space between the option and the extension are optional. | ||
| -fs | specifies a directory for the output files. For example, to place the .abs file generated by the absolute lister in C:\ABSDIR use this command: abs2000 -fs C:\ABSDIR filename.outIf the -fs option is not specified, the absolute lister generates the .abs files in the current directory. |
|
| -q | (quiet) suppresses the banner and all progress information. | |
| input file | names the linked object file. If you do not supply an extension, the absolute lister assumes that the input file has the default extension .out. If you do not supply an input filename when you invoke the absolute lister, the absolute lister prompts you for one. | |
The absolute lister produces an output file for each file that was linked. These files are named with the input filenames and an extension of .abs. Header files, however, do not generate a corresponding .abs file.
Assemble these files with the --absolute_listing assembler option as follows to create the absolute listing:
cl2000 --absolute_listing filename .abs
The -e options affect both the interpretation of filenames on the command line and the names of the output files. They should always precede any filename on the command line.
The -e options are useful when the linked object file was created from C files compiled with the debugging option (--symdebug:dwarf compiler option). When the debugging option is set, the resulting linked object file contains the name of the source files used to build it. In this case, the absolute lister does not generate a corresponding .abs file for the C header files. Also, the .abs file corresponding to a C source file uses the assembly file generated from the C source file rather than the C source file itself.
For example, suppose the C source file hello.csr is compiled with the debugging option set; the debugging option generates the assembly file hello.s. The hello.csr file includes hello.hsr. Assuming the executable file created is called hello.out, the following command generates the proper .abs file:
abs2000 -ea s -ec csr -eh hsr hello.out
An .abs file is not created for hello.hsr (the header file), and hello.abs includes the assembly file hello.s, not the C source file hello.csr.
9.3 Absolute Lister Example
This example uses three source files. The files module1.asm and module2.asm both include the file globals.def.
module1.asm
.text
array .usect ".ebss",100
dflag .usect ".ebss", 2
.copy globals.def
MOV ACC, #offset
MOV ACC, #dflag
module2.asm
offset .usect ".ebss", 2
.copy globals.def
MOV ACC, #offset
MOV ACC, #array
globals.def
.global dflag
.global array
.global offset
The following steps create absolute listings for the files module1.asm and module2.asm:
| Step 1: | First, assemble module1.asm and module2.asm: cl2000 module1This creates two object files called module1.obj and module2.obj. |
| Step 2: | Next, link module1.obj and module2.obj using the following linker command file, called bttest.cmd: |
--output_file=bttest.out
--map_file=bttest.map
module1.obj
module2.obj
MEMORY
{
PAGE 0: ROM: origin=2000h length=2000h
PAGE 1: RAM: origin=8000h length=8000h
}
SECTIONS
{
.data: >RAM
.text: >ROM
.ebss: >RAM
}
Invoke the linker: cl2000 --run_linker bttest.cmdThis command creates an executable object file called bttest.out; use this file as input for the absolute lister. |
|
| Step 3: | Now, invoke the absolute lister: abs2000 bttest.outThis command creates two files called module1.abs and module2.abs: module1.abs: |
.nolist
array .setsym 000008000h
dflag .setsym 000008064h
offset .setsym 000008066h
.data .setsym 000008000h
edata .setsym 000008000h
.text .setsym 000002000h
etext .setsym 000002008h
.usect .setsym 000008000h
end .setsym 000008068h
.setsect ".text",000002000h
.setsect ".data",000008000h
.setsect ".ebss",00008000h
.list
.text
.copy "module1.asm"
| module2.abs: |
.nolist
array .setsym 000008000h
dflag .setsym 000008064h
offset .setsym 000008066h
.data .setsym 000008000h
edata .setsym 000008000h
.text .setsym 000002000h
etext .setsym 000002008h
.usect .setsym 000008000h
end .setsym 000008068h
.setsect ".text",000002004h
.setsect ".data",000008000h
.setsect ".ebss",00008066h
.list
.text
.copy "module2.asm"
These files contain the following information that the assembler needs for Step 4:
The .setsym and .setsect directives are useful only for creating absolute listings, not normal assembly. |
|
| Step 4: | Finally, assemble the .abs files created by the absolute lister (remember that you must use the --absolute_listing option when you invoke the assembler): cl2000 --absolute_listing module1.absThis command sequence creates two listing files called module1.lst and module2.lst; no object code is produced. These listing files are similar to normal listing files; however, the addresses shown are absolute addresses. The absolute listing files created are module1.lst (see Example 9-1 ) and module2.lst (see Example 9-2). |
Example 9-1 module1.lst
module1.abs PAGE 1
15 002000 .text
16 .copy "module1.asm" 1 002000 .text
2 008000 array .usect ".ebss",100
3 008064 dflag .usect ".ebss",2
4 .copy globals.def
1 .global dflag
2 .global array
3 .global offset
5 002000 FF20! MOV ACC,#offset
002001 8066
6 002002 FF20- MOV ACC,#dflag
002003 8064
Copyright© 2018, Texas Instruments Incorporated. An IMPORTANT NOTICE for this document addresses availability, warranty, changes, use in safety-critical applications, intellectual property matters and other important disclaimers.